This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3235MODSF: UART programming using CH340 and SmartRF flash programmer 2(version 1.8.0)

Part Number: CC3235MODSF
Other Parts Discussed in Thread: LAUNCHCC3235MOD, UNIFLASH

We have designed Wifi board using the module CC3235MODSF. Unfortunately there is no availability of LAUNCHCC3235MOD evaluation kit to program the board using UART.

Can i use CH340 and SmartRF flash programmer 2 instead to program the CC3235MODSF ?

If not, please suggest us what else can be used to program ?

Regards,

Vasanth M

  • Hi Vasanth,

    Although on the launchpad you can load program using the USB interface and the Uniflash tool, the following options can be used as well:

    For further details refer to the CC3235MODx Product Line Guide here.

    To test the RF of our C3xxx devices it is suggested to use Uniflash and Radio Tool, not "SmartRF Flash Programmer".  

    Note that the top half of the launchpad is a XDS110 JTAG emulator the same as this one, but you can use another tool to have a UART interface.

    BR,

    Jessica M. Torres