This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

wlan_cu messages does not stop appearing when configured for ad-hoc mode



Hi,

I've configured my TiWi using the command:

However, after doing so I get these messages popping up:

TIWLAN: 3513.456577: %%%%%%%    SELF SELECT SUCCESS, bssid: 02.00.00.65.fa.f8 %%%%%%%

TIWLAN: 3525.156909: %%%%%%%    SELF SELECT SUCCESS, bssid: 02.00.00.65.fa.f9 %%%%%%%

...

TIWLAN: 3540.366891: %%%%%%%    SELF SELECT SUCCESS, bssid: 02.00.00.65.fa.fa %%%%%%%

How do I stop that from happening?

  • Hi Grant,

    The message indicates that the TiWi has created an Ad-hoc network and no other station has  associated yet with the network. Once a second station joins the network the messages will not be displayed.

    Regards,

    Sinoj