Dear
Our team use WL1837MOD as AP, and 2.4GHz is setted.
I want to know that whether the parameter of channel is affective for 2.4GHz ?
------------------------------------------------------------ the follow is a part of hostapd.conf ----------------------
# Channel number (IEEE 802.11)
# (default: 0, i.e., not set)
# Please note that some drivers do not use this value from hostapd and the
# channel will need to be configured separately with iwconfig.
# When set to 0, automatic channel selection will be engaged. A channel
# will be selected from the desired hw_mode.
channel=0
-------------------------------------------------------------
Yunxue Wang