This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1807MOD: Repeat MLME-AUTHENTICATE/DEAUTHENTICATE

Part Number: WL1807MOD

Hello,

With 8 STAs connected to the WL1807 AP, All STAs repeat MLME-AUTHENTICATE/DEAUTHENTICATE.

This problem continues until turn off/on wlan interface (ip link set wlan1 down/up).

I have only met this problem twice, so it is difficult to parse.

Could you tell me a solution of this issue or a similar issue?

Regards,

tail -n 100 /var/log/messages
[2022-09-20 20:07:58.603] Sep 20 20:07:29 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:b2:17 MLME: MLME-DELETEKEYS.request(xx:xx:xx:xx:b2:17)
[2022-09-20 20:07:58.964] Sep 20 20:07:29 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 IEEE 802.11: authentication OK (open system)
[2022-09-20 20:07:58.964] Sep 20 20:07:29 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 MLME: MLME-AUTHENTICATE.indication(xx:xx:xx:xx:ba:d4, OPEN_SYSTEM)
[2022-09-20 20:07:58.964] Sep 20 20:07:29 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 MLME: MLME-DELETEKEYS.request(xx:xx:xx:xx:ba:d4)
[2022-09-20 20:07:58.964] Sep 20 20:07:30 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:b2:4c IEEE 802.11: authentication OK (open system)
[2022-09-20 20:07:58.964] Sep 20 20:07:30 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:b2:4c MLME: MLME-AUTHENTICATE.indication(xx:xx:xx:xx:b2:4c, OPEN_SYSTEM)
[2022-09-20 20:07:58.964] Sep 20 20:07:30 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:b2:4c MLME: MLME-DELETEKEYS.request(xx:xx:xx:xx:b2:4c)
[2022-09-20 20:07:58.964] Sep 20 20:07:30 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:b2:17 IEEE 802.11: deauthenticated
[2022-09-20 20:07:58.978] Sep 20 20:07:30 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:b2:17 MLME: MLME-DEAUTHENTICATE.indication(xx:xx:xx:xx:b2:17, 3)
[2022-09-20 20:07:58.978] Sep 20 20:07:30 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:b2:17 MLME: MLME-DELETEKEYS.request(xx:xx:xx:xx:b2:17)
[2022-09-20 20:07:58.978] Sep 20 20:07:30 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:b2:17 IEEE 802.11: authentication OK (open system)
[2022-09-20 20:07:58.978] Sep 20 20:07:30 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:b2:17 MLME: MLME-AUTHENTICATE.indication(xx:xx:xx:xx:b2:17, OPEN_SYSTEM)
[2022-09-20 20:07:58.978] Sep 20 20:07:30 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:b2:17 MLME: MLME-DELETEKEYS.request(xx:xx:xx:xx:b2:17)
[2022-09-20 20:07:58.978] Sep 20 20:07:30 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 IEEE 802.11: deauthenticated
[2022-09-20 20:07:58.978] Sep 20 20:07:30 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 MLME: MLME-DEAUTHENTICATE.indication(xx:xx:xx:xx:ba:d4, 3)
[2022-09-20 20:07:58.978] Sep 20 20:07:30 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 MLME: MLME-DELETEKEYS.request(xx:xx:xx:xx:ba:d4)
[2022-09-20 20:07:58.995] Sep 20 20:07:30 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 IEEE 802.11: authentication OK (open system)
[2022-09-20 20:07:58.995] Sep 20 20:07:30 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 MLME: MLME-AUTHENTICATE.indication(xx:xx:xx:xx:ba:d4, OPEN_SYSTEM)
[2022-09-20 20:07:58.995] Sep 20 20:07:30 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 MLME: MLME-DELETEKEYS.request(xx:xx:xx:xx:ba:d4)
[2022-09-20 20:07:58.995] Sep 20 20:07:30 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:b2:17 IEEE 802.11: authentication OK (open system)
[2022-09-20 20:07:58.995] Sep 20 20:07:30 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:b2:17 MLME: MLME-AUTHENTICATE.indication(xx:xx:xx:xx:b2:17, OPEN_SYSTEM)
[2022-09-20 20:07:58.995] Sep 20 20:07:30 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:b2:17 MLME: MLME-DELETEKEYS.request(xx:xx:xx:xx:b2:17)
[2022-09-20 20:07:58.995] Sep 20 20:07:31 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 IEEE 802.11: authentication OK (open system)
[2022-09-20 20:07:58.997] Sep 20 20:07:31 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 MLME: MLME-AUTHENTICATE.indication(xx:xx:xx:xx:ba:d4, OPEN_SYSTEM)
[2022-09-20 20:07:58.998] Sep 20 20:07:31 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 MLME: MLME-DELETEKEYS.request(xx:xx:xx:xx:ba:d4)
[2022-09-20 20:07:58.998] Sep 20 20:07:31 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 IEEE 802.11: deauthenticated
[2022-09-20 20:07:58.998] Sep 20 20:07:31 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 MLME: MLME-DEAUTHENTICATE.indication(xx:xx:xx:xx:ba:d4, 3)
[2022-09-20 20:07:58.998] Sep 20 20:07:31 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 MLME: MLME-DELETEKEYS.request(xx:xx:xx:xx:ba:d4)
[2022-09-20 20:07:58.998] Sep 20 20:07:31 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 IEEE 802.11: authentication OK (open system)
[2022-09-20 20:07:58.998] Sep 20 20:07:31 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 MLME: MLME-AUTHENTICATE.indication(xx:xx:xx:xx:ba:d4, OPEN_SYSTEM)
[2022-09-20 20:07:59.310] Sep 20 20:07:31 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 MLME: MLME-DELETEKEYS.request(xx:xx:xx:xx:ba:d4)
[2022-09-20 20:07:59.310] Sep 20 20:07:32 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 IEEE 802.11: authentication OK (open system)
[2022-09-20 20:07:59.310] Sep 20 20:07:32 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 MLME: MLME-AUTHENTICATE.indication(xx:xx:xx:xx:ba:d4, OPEN_SYSTEM)
[2022-09-20 20:07:59.310] Sep 20 20:07:32 imx6ull14x14evk daemon.debug hostapd: wlan1: STA xx:xx:xx:xx:ba:d4 MLME: MLME-DELETEKEYS.request(xx:xx:xx:xx:ba:d4)