Other Parts Discussed in Thread: WL1837
Dear
About the process of updating wl18xx firmware data,I have a few different understandings, and please help me to confirm which one is right as following:
# some wifi modules which are associated with wifi firmware have been updated in kernel before updating firmware.
① I copy the new firmware (such as wl18xx-fw-4.bin) to /lib/firmware/ti-connectivity/, then re-run configure_device.sh only once time,some parametar(such as 2.4GHz or 5GHz) will be update to the wl18xx-fw-4.bin, at the last, reboot system, the new data of firmware will be reloaded to wl1837 by SDIO interface after rebooting system.
② I copy the new firmware (such as wl18xx-fw-4.bin) to /lib/firmware/ti-connectivity/, then re-run configure_device.sh,but reboot isn’t needed,the lastest parameter of firmware will be reloaded immediately to wl1837 by SDIO interface。
If both are wrong, please introduce the process about updating data of firmware.
Thanks
Yunxue Wang