This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1807MOD: 4addr mode support

Part Number: WL1807MOD

Hello,

I’m trying to set a Wifi-Ethernet bridge with AP/Clients connection and each client is bridged to a wired network behind. I’m using WL1807 module with FW (Rev 8.9.0.0.83) and trying to use 4addr mode:

On STA side, I set up the interface with 4addr mode:  iw dev wlan0 set 4addr on

And bridge the 4-addr mode client interface: brctl addif br_lan wlan0

On AP side, I added to my hostapd configuration:

 wds_sta=1

wds_bridge=br0

When 4addr client connects, an interface should be created (wlan0.sta0,…) but it is not the case and client machine can’t ping AP and IPs bridged behind.

So, 4addr mode is supported on AP and STA ? and if it does, what I’m missing ?

Thanks,

Hmaied