Hi,
using Raymond's driver from this thread, https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/855716/msp432p4111-spi-master-ping-pong-dma-rx/3172831?tisearch=e2e-sitesearch&keymatch=ping%20pong#3172831 I was able to implement PingPong Mode on the CC3235SF. The transmission of an image seems to work without errors. However, the problems start when I want to send the received data via my websocket connection. Here I regularly get the abort error [ERROR] - FATAL ERROR: Driver Abort detected. From my send_len = (int)sl_Send((int)socket, buffer, (int)len, 0); i recieve error -2005. If I send data via websocket without using the SPI the problem does not occur. I suspect that the NWP has some kind of problem with the modified driver. Please give me some hints on how to tackle the problem. Thank you in advance.