This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220SF: Problems reconnecting to Wi-Fi

Part Number: CC3220SF

Hi,

I'm using the CC3220SF for a Smart Garage door opener gadget to open and close the door remotely with an app, I'm getting the problem that after 2-3 days or a couple of weeks the device loses connection to wifi and can't reconnect automatically to WiFi, it needs to be power cycled and it reconnects automatically but the problem repeats again after a week or so.

I logged what the CC3220 was printing on the serial port during the failure and it printed: 

FATAL ERROR: Driver Abort detected

Error Read: -2005

  1. What could be causing these problems?
  2. What can be done to solve this issue?

Thanks