Other Parts Discussed in Thread: UNIFLASH
We are having some issues between our CM and how they program the CC3235MODSF and the way we program it.
Basically BD(we) are programming it using the UART interface with an .sli file using the batch process with an FTDI cable. This works for us and also works for our CM.
The CM though wanted to goto a offline programming method and they have implemented it but it has lead to a problem in that the MAC address is no longer readable.
The offline method they are using is they converted our .sli file to a .bin file and programmed the flash inside the CC3235MODSF through the external pins that come out of the module.
So we think the issue maybe that there are other registers that need to be setup inside the CC3235MODSF that is not done by just programming the internal flash.
Can you help with the questions in the powerpoint and a few others?
- What does the *.sli include that is not in the *.bin file?
- Is there a way to program all the registers that are needed through the external SPI interface?
Thank you