This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200: lost connection in station mode

Part Number: CC3200


I've connected a cc3200 in station mode to an accesspoint. An app is connected to the same accesspoint and has successfully connected to the CC3200 via it:

CC3200 <---> accesspoint <---> App

If I disconnect the wifi connection between the accesspoint and the app, I'm not able to detect this on the CC3200 side: 

CC3200 <---> accesspoint <-X-> App

Is there an event, status, ... that signals me the shown connection loss at the CC3200 side from the accesspoint?

(The SL_WLAN_STA_DISCONNECTED_EVENT for example is only triggered when the CC3200 is disconnected from the accesspoint and not in the case shown.)