Hello TI Team,
I'm developing an application that intends to do the following:
- configure one LaunchXL-CC3235S as an Access Point and another one as Station.
- transmit data between AP and STA (full duplex, bidirectional) on continuous basis.
for these two requirements, I've developed attached applications. With the same, I facing following issues:
- Transmission speeds seems to be very slow. I'm getting almost one message per second. Can something be done for that? My minimum requirements is of 4 Mbps. How do I increase the data rate and how do I verify the same?
- My socket_task in the program has random execution. Sometimes is sends 577 messages, sometimes 5444 sometimes 389. (I've tried three iterations) This shall be continuous. As I've written two counters, it should run 50000 x 50000 times without stopping or switching. I'm not able to understand why does the program stops current execution and switches back to main_thread task?

/*
* ======== main_freertos.c ========
*/
#include <stdint.h>
/* POSIX Header files */
#include <pthread.h>
/* RTOS header files */
#include "FreeRTOS.h"
#include "task.h"
/* TI-DRIVERS Header files */
#include "ti_drivers_config.h"
/* TI-RTOS Header files */
#include <ti/drivers/GPIO.h>
extern void * mainThread(void *arg0);
/* Stack size in bytes */
#define THREADSTACKSIZE 1024
/*
* ======== main ========
*/
int main(void)
{
pthread_t thread;
pthread_attr_t pAttrs;
struct sched_param priParam;
int retc = 0;
int detachState;
/* Call board init functions */
Board_init();
retc = xTaskCreate( mainThread, /* Pointer to the function that implements the task. */
"mainThread 1",/* Text name for the task. This is to facilitate debugging only. */
THREADSTACKSIZE, /* Stack depth - small microcontrollers will use much less stack than this. */
NULL, /* This example does not use the task parameter. */
3, /* This task will run at Maximum priority. */
NULL ); /* This example does not use the task handle. */
if(retc != pdPASS)
{
printf("\n\n");
printf("Main Task Creation failed!!!");
printf("\n\n");
while(1)
{
;
}
}
if(retc == pdPASS)
{
printf("\n\n");
printf("Main Task Creation Succeeded !!!");
printf("\n\n");
}
/* Start the FreeRTOS scheduler */
vTaskStartScheduler();
return (0);
}
void vApplicationMallocFailedHook()
{
/* Handle Memory Allocation Errors */
while(1)
{
}
}
void vApplicationStackOverflowHook(TaskHandle_t pxTask,
char *pcTaskName)
{
//Handle FreeRTOS Stack Overflow
while(1)
{
}
}
void vApplicationTickHook(void)
{
}
void vPreSleepProcessing(uint32_t ulExpectedIdleTime)
{
}
void
vApplicationIdleHook(void)
{
/* Handle Idle Hook for Profiling, Power Management etc */
}
#if defined (__GNUC__)
void * _sbrk(uint32_t delta)
{
extern char _end; /* Defined by the linker */
extern char __HeapLimit;
static char *heap_end;
static char *heap_limit;
char *prev_heap_end;
if(heap_end == 0)
{
heap_end = &_end;
heap_limit = &__HeapLimit;
}
prev_heap_end = heap_end;
if(prev_heap_end + delta > heap_limit)
{
return((void *) -1L);
}
heap_end += delta;
return((void *) prev_heap_end);
}
#endif
#include <ti/drivers/net/wifi/simplelink.h>
#include <ti/drivers/net/wifi/slnetifwifi.h>
#include <ti/display/Display.h>
#include <ti/drivers/SPI.h>
#include "FreeRTOS.h"
#include "task.h"
// TI-Driver includes
#include "ti_drivers_config.h"
#include "pthread.h"
#include <string.h>
#include <stdint.h>
/* BSD support */
#include <netinet/in.h>
#include <arpa/inet.h>
#include <sys/socket.h>
#include <sys/select.h>
#include <ti/net/slnetutils.h>
#define DEVICE_ERROR ("Device error, please refer \"DEVICE ERRORS CODES\" section in errors.h")
#define WLAN_ERROR ("WLAN error, please refer \"WLAN ERRORS CODES\" section in errors.h")
#define SL_STOP_TIMEOUT (200)
#define UDPPORT (1000)
#define SPAWN_TASK_PRIORITY (9)
#define TASK_STACK_SIZE (2048)
#define SLNET_IF_WIFI_PRIO (5)
#define SLNET_IF_WIFI_NAME "CC32xx"
#define UDPPACKETSIZE 256
#define THREADSTACKSIZE 4096
#define SSID_NAME "HCTRIVEDI_AP1" // AP SSID
// #define SECURITY_TYPE SL_WLAN_SEC_TYPE_WPA_WPA2 // Security type could be SL_WLAN_SEC_TYPE_OPEN
_u8 SECURITY_TYPE = SL_WLAN_SEC_TYPE_WPA_WPA2;
#define SECURITY_KEY "HarshAPConnect" // Password of the secured AP
#define device_name "Trivedi" // set new name of the device
#define country_code "US" // setting country code...
#define ApPower 15 // set Tx power level
_u8 status = 0;
_u8 flag_second_ping = 0;
static _u32 retc = 0;
pthread_t udpThread = (pthread_t)NULL;
pthread_t spawn_thread = (pthread_t)NULL;
int32_t mode;
Display_Handle display;
char msg1[26], msg2[6], msg3[6];
/*
* ======== printError ========
*/
void printError(char *errString, int code)
{
Display_printf(display, 0, 0, "Error! code = %d, Description = %s\n", code, errString);
while(1);
}
void SimpleLinkNetAppEventHandler(SlNetAppEvent_t *pNetAppEvent)
{
// unused in this application...
}
void SimpleLinkFatalErrorEventHandler(SlDeviceFatal_t *slFatalErrorEvent)
{
/* Unused in this application */
}
void SimpleLinkNetAppRequestMemFreeEventHandler(uint8_t *buffer)
{
/* Unused in this application */
}
void SimpleLinkNetAppRequestEventHandler(SlNetAppRequest_t *pNetAppRequest, SlNetAppResponse_t *pNetAppResponse)
{
/* Unused in this application */
}
void SimpleLinkHttpServerEventHandler(SlNetAppHttpServerEvent_t *pHttpEvent, SlNetAppHttpServerResponse_t *pHttpResponse)
{
/* Unused in this application */
}
void SimpleLinkWlanEventHandler(SlWlanEvent_t *pWlanEvent)
{
if(pWlanEvent == NULL)
{
return;
}
switch(pWlanEvent->Id)
{
case SL_WLAN_EVENT_STA_ADDED:
printf("\n\n A station with following parameters has got connected to the AP: %s", (signed char*)SSID_NAME);
printf("\n\n %02x:%02x:%02x:%02x:%02x:%02x \n\n",
pWlanEvent->Data.STAAdded.Mac[0],
pWlanEvent->Data.STAAdded.Mac[1],
pWlanEvent->Data.STAAdded.Mac[2],
pWlanEvent->Data.STAAdded.Mac[3],
pWlanEvent->Data.STAAdded.Mac[4],
pWlanEvent->Data.STAAdded.Mac[5]);
// code to get the number of connected stations...
_u8 num_ap_connected_sta;
_u16 len = sizeof(num_ap_connected_sta);
status = sl_NetCfgGet(SL_NETCFG_AP_STATIONS_NUM_CONNECTED, NULL, &len, &num_ap_connected_sta);
printf("Revised number of connected stations = %d\n", num_ap_connected_sta);
// code to get the list of stations...
SlNetCfgStaInfo_t ApStaList[4];
_u8 sta_info_len = sizeof(ApStaList);
_u8 start_sta_index = 0;
_u8 actual_num_sta, ii;
sl_NetCfgGet(SL_NETCFG_AP_STATIONS_INFO_LIST, &start_sta_index, &sta_info_len, (_u8 *)ApStaList);
actual_num_sta = sta_info_len / sizeof(SlNetCfgStaInfo_t);
printf("\n \n Actual num_stations = %d", actual_num_sta);
printf("\n \n upon sta_info_len = %d", sta_info_len);
for (ii=0; ii<actual_num_sta; ii++)
{
SlNetCfgStaInfo_t *staInfo = &ApStaList[ii];
printf(" Ap Station %d is connected\n", ii);
printf(" NAME: %s\n", staInfo->Name);
printf(" MAC: %02x:%02x:%02x:%02x:%02x:%02x\n", staInfo->MacAddr[0], staInfo->MacAddr[1], staInfo->MacAddr[2], staInfo->MacAddr[3], staInfo->MacAddr[4], staInfo->MacAddr[5]);
printf(" IP: %d.%d.%d.%d\n", SL_IPV4_BYTE(staInfo->Ip,3), SL_IPV4_BYTE(staInfo->Ip,2), SL_IPV4_BYTE(staInfo->Ip,1), SL_IPV4_BYTE(staInfo->Ip,0));
// Display_printf(display, 0, 0,"\n\r NAME: %s\n\r", staInfo->Name);
// Display_printf(display, 0, 0,"\n\r IP: %d.%d.%d.%d\n", SL_IPV4_BYTE(staInfo->Ip,3), SL_IPV4_BYTE(staInfo->Ip,2), SL_IPV4_BYTE(staInfo->Ip,1), SL_IPV4_BYTE(staInfo->Ip,0));
SlNetCfgIpV4Args_t *staInfo2 = &ApStaList[ii];
printf(" Gateway: %d.%d.%d.%d\n\n", SL_IPV4_BYTE(staInfo2->IpGateway,3),SL_IPV4_BYTE(staInfo2->IpGateway,2),SL_IPV4_BYTE(staInfo2->IpGateway,1),SL_IPV4_BYTE(staInfo2->IpGateway,0));
}
break;
case SL_WLAN_EVENT_STA_REMOVED:
printf("\n\n A station with following parameters have been removed from the AP: %s", (signed char*)SSID_NAME);
printf("\n\n %02x:%02x:%02x:%02x:%02x:%02x \n\n",
pWlanEvent->Data.STARemoved.Mac[0],
pWlanEvent->Data.STARemoved.Mac[1],
pWlanEvent->Data.STARemoved.Mac[2],
pWlanEvent->Data.STARemoved.Mac[3],
pWlanEvent->Data.STARemoved.Mac[4],
pWlanEvent->Data.STARemoved.Mac[5]);
break;
default:
break;
}
printf("\n");
printf("out of WLAN Event Handler Switch statement ...");
printf("\n");
retc = 940;
}
void SimpleLinkGeneralEventHandler(SlDeviceEvent_t *pDevEvent)
{
/* Unused in this application */
}
void SimpleLinkSockEventHandler(SlSockEvent_t *pSock)
{
/* Unused in this application */
}
void check_device_initial_mode(void)
{
mode = sl_Start(0, 0, 0);
Display_printf(display, 0, 0,"\n\rMode: %d", mode);
if (mode < 0)
{
Display_printf(display, 0, 0,"\n\r[line:%d, error code:%d] %s\n\r", __LINE__, mode, DEVICE_ERROR);
}
switch(mode)
{
case 0:
printf("Role = Station \n");
break;
case 1:
printf("Role = Reserved! \n");
break;
case 2:
printf("Role = Access Point \n");
break;
case 3:
printf("Role = ROLE_P2P \n");
break;
case 4:
printf("Role = ROLE_TAG \n");
break;
default:
printf("Some Error Occured! No such role!! \n");
break;
}
}
void configure_AP_mode(void)
{
if(mode != ROLE_AP)
{
/* Set NWP role as STA */
mode = sl_WlanSetMode(ROLE_AP);
if (mode < 0)
{
printf("\n AP Mode could not be configfured!! \n");
}
/* For changes to take affect, we restart the NWP */
status = sl_Stop(SL_STOP_TIMEOUT);
if (status < 0)
{
printf("Device could not be stopped post mode change!! \n");
}
mode = sl_Start(0, 0, 0);
if (mode < 0)
{
printf("Device could not be restarted post mode change!! \n");
}
}
}
void AP_configuration(void)
{
if(mode == ROLE_AP)
{
printf("Device successfully configured to %d mode (i.e. AP Mode) \n", mode);
}
if(mode == ROLE_AP)
{
printf("Configuring AP parameters now... \n");
// as per response from TI post, there is no need to restart the device after every change. Hence, keeping only a single restart at the end of this if statement.
// set device name
status = sl_NetAppSet (SL_NETAPP_DEVICE_ID,SL_NETAPP_DEVICE_URN, strlen(device_name), (signed char*)device_name);
if( status )
{
printf("Device Name Could not be Updated \n");
}
else
{
printf("Device Name Updated \n");
}
// set SSID for the AP
status = sl_WlanSet(SL_WLAN_CFG_AP_ID, SL_WLAN_AP_OPT_SSID, strlen(SSID_NAME), (signed char*)SSID_NAME);
if(status)
{
printf("SSID Could not be Updated \n");
}
else
{
printf("SSID Name Updated \n");
}
// set country code for AP
status = sl_WlanSet(SL_WLAN_CFG_GENERAL_PARAM_ID, SL_WLAN_GENERAL_PARAM_OPT_COUNTRY_CODE, 2, (signed char*)country_code);
if(status)
{
printf("Device Country Code could not be updated \n");
}
else
{
printf("Device Country Code updated \n");
}
// set security settings
status = sl_WlanSet(SL_WLAN_CFG_AP_ID, SL_WLAN_AP_OPT_SECURITY_TYPE, 1, (_u8 *)&SECURITY_TYPE);;
if(status)
{
Display_printf(display, 0, 0, "Security Type could not be updated");
}
else
{
printf("Device Security Settings updated \n");
}
// set password for updated security type
status = sl_WlanSet(SL_WLAN_CFG_AP_ID, SL_WLAN_AP_OPT_PASSWORD, strlen(SECURITY_KEY), (signed char*)SECURITY_KEY);
if(status)
{
Display_printf(display, 0, 0, "Security Type could not be updated");
}
else
{
printf("Device Security Password updated \n");
}
// set Tx power levels => 0 dB backoff for now
status = sl_WlanSet(SL_WLAN_CFG_GENERAL_PARAM_ID, SL_WLAN_GENERAL_PARAM_OPT_AP_TX_POWER,1,(signed char*)ApPower);
if(status)
{
printf("Device power level could not be updated \n");
}
else
{
printf("Device power updated \n");
}
/* For changes to take affect, we restart the NWP */
status = sl_Stop(SL_STOP_TIMEOUT);
if (status < 0)
{
printf("Device could not be stopped post mode change!! \n");
}
mode = sl_Start(0, 0, 0);
if (mode < 0)
{
printf("Device could not be restarted post mode change!! \n");
}
else
{
printf("Device restarted successfully post AP settings and mode configurations !! \n\n\n");
}
}
}
void config_network_parameters(void)
{
printf("Configuring Network Parameters now... \n");
SlNetCfgIpV4Args_t ipV4;
ipV4.Ip = (_u32)SL_IPV4_VAL(10,1,1,200); // IP address
ipV4.IpMask = (_u32)SL_IPV4_VAL(255,255,255,0); // Subnet mask
ipV4.IpGateway = (_u32)SL_IPV4_VAL(10,1,1,1); // Default gateway address
ipV4.IpDnsServer = (_u32)SL_IPV4_VAL(8,16,32,64); // _u32 DNS server address
status = sl_NetCfgSet(SL_NETCFG_IPV4_AP_ADDR_MODE,SL_NETCFG_ADDR_STATIC,sizeof(SlNetCfgIpV4Args_t), (_u8 *)&ipV4);
if(status)
{
printf("Network Parameters Could not be Updated ... \n");
}
else
{
printf("Network Parameters Updated Successfully ... \n");
}
}
void get_device_config_parameters(void)
{
printf("Getting device configuration parameters through get_device_config_parameters function!! \n\n");
_u8 macAddressVal[SL_MAC_ADDR_LEN];
_u16 macAddressLen = SL_MAC_ADDR_LEN;
_u16 ConfigOpt1 = 0;
sl_NetCfgGet(SL_NETCFG_MAC_ADDRESS_GET,&ConfigOpt1,&macAddressLen,(_u8 *)macAddressVal);
printf("AP MAC address is: %02x:%02x:%02x:%02x:%02x:%02x \n ", macAddressVal[0], macAddressVal[1], macAddressVal[2], macAddressVal[3], macAddressVal[4], macAddressVal[5]);
_u16 len = sizeof(SlNetCfgIpV4Args_t);
_u16 ConfigOpt2 = 0; //return value could be one of the following: SL_NETCFG_ADDR_DHCP / SL_NETCFG_ADDR_DHCP_LLA / SL_NETCFG_ADDR_STATIC
SlNetCfgIpV4Args_t ipV4 = {0};
sl_NetCfgGet(SL_NETCFG_IPV4_AP_ADDR_MODE,&ConfigOpt2,&len,(_u8 *)&ipV4);
printf("DHCP is %s \n\r IP %d.%d.%d.%d \n\r MASK %d.%d.%d.%d \n\r GW %d.%d.%d.%d \n\r DNS %d.%d.%d.%d \n",
(ConfigOpt2 == SL_NETCFG_ADDR_DHCP) ? "ON" : "OFF",
SL_IPV4_BYTE(ipV4.Ip,3),SL_IPV4_BYTE(ipV4.Ip,2),SL_IPV4_BYTE(ipV4.Ip,1),SL_IPV4_BYTE(ipV4.Ip,0),
SL_IPV4_BYTE(ipV4.IpMask,3),SL_IPV4_BYTE(ipV4.IpMask,2),SL_IPV4_BYTE(ipV4.IpMask,1),SL_IPV4_BYTE(ipV4.IpMask,0),
SL_IPV4_BYTE(ipV4.IpGateway,3),SL_IPV4_BYTE(ipV4.IpGateway,2),SL_IPV4_BYTE(ipV4.IpGateway,1),SL_IPV4_BYTE(ipV4.IpGateway,0),
SL_IPV4_BYTE(ipV4.IpDnsServer,3),SL_IPV4_BYTE(ipV4.IpDnsServer,2),SL_IPV4_BYTE(ipV4.IpDnsServer,1),SL_IPV4_BYTE(ipV4.IpDnsServer,0));
printf("\n");
printf("\n");
}
// ping activation
void ping_first_success(void)
{
SlNetAppPingReport_t report; // report structure that will be available at the end of ping
SlNetAppPingCommand_t pingCommand;
pingCommand.Ip = SL_IPV4_VAL(10,1,1,201); // destination IP address is 10.1.1.200
pingCommand.PingSize = 150; // size of ping, in bytes
pingCommand.PingIntervalTime = 100; // delay between pings, in milliseconds
pingCommand.PingRequestTimeout = 1000; // timeout for every ping in milliseconds
pingCommand.TotalNumberOfAttempts = 50; // number of ping requests
pingCommand.Flags = 2; // report at the end of first successful ping.
status = sl_NetAppPing( &pingCommand, SL_AF_INET, &report, NULL );
if (status)
{
printf("\n\r ~~~~~ Ping Failure!! ~~~~~");
}
printf("\n");
while(report.PacketsReceived != 1) {}
}
void ping_second_confirmation(void)
{
// This function verifies that the connection is still there and then data transfer is initiated.
// ping_first_success function returns upon first siccessful ping. While this function sends 20 pings and ensures 90 % success before creating and connecting the socket.
SlNetAppPingReport_t report; // report structure that will be available at the end of ping
SlNetAppPingCommand_t pingCommand;
pingCommand.Ip = SL_IPV4_VAL(10,1,1,201); // destination IP address is 10.1.1.200
pingCommand.PingSize = 150; // size of ping, in bytes
pingCommand.PingIntervalTime = 100; // delay between pings, in milliseconds
pingCommand.PingRequestTimeout = 1000; // timeout for every ping in milliseconds
pingCommand.TotalNumberOfAttempts = 50; // number of ping requests
pingCommand.Flags = 0; // report at the end of first successful ping
status = sl_NetAppPing( &pingCommand, SL_AF_INET, &report, NULL );
if (status)
{
printf("\n\r ~~~~~ Ping Failure!! ~~~~~");
}
printf("\n");
if(report.PacketsReceived >= 45)
{
printf("\n\r 90%% pings were successfully returned...");
printf("\n\r Connection can be assumed rock solid ;) ");
printf("\n\r Socket creation and connection can be processed now...");
printf("\n");
}
else
{
unsigned char ping_success_rate = 0;
ping_success_rate = ((1-((report.PacketsReceived-report.PacketsSent)/report.PacketsSent))*100);
printf("\n \r Ping success rate is %d, reconnection shall be done before creating and connecting a socket!!", ping_success_rate);
printf("\n");
while(1);
}
flag_second_ping = 1;
}
void socket_task(void *pvParameters)
{
long counter1 = 0;
long counter2 = 0;
unsigned char status_socket = 0;
_i16 Sd;
SlSockAddrIn_t Addr;
_i8 SendBuf[] = "Hello from AP !!!";
_i8 RecvBuf[1460] ={0};
Sd = sl_Socket(SL_AF_INET, SL_SOCK_DGRAM, 0); // IPv4 socket (UDP, TCP, etc), UDP Packets, Null
if( Sd < 0 )
{
printf("Socket opening failed!!");
}
Addr.sin_family = SL_AF_INET;
Addr.sin_port = sl_Htons(5001);
Addr.sin_addr.s_addr = SL_INADDR_ANY; // bind to any address
// Addr.sin_addr.s_addr = sl_Htonl(SL_IPV4_VAL(192,168,1,31)); // bind to this specific address only.
status_socket = sl_Bind(Sd, ( SlSockAddr_t *)&Addr, sizeof(SlSockAddrIn_t));
if(status_socket)
{
printf("\n\n\n Socket Binding failed");
}
else
{
printf("\n socket binding completed \n");
}
Addr.sin_addr.s_addr = sl_Htonl(SL_IPV4_VAL(10,1,1,201)); // connect with this specific address only.
status_socket = sl_Connect(Sd, ( SlSockAddr_t *)&Addr, sizeof(SlSockAddrIn_t)); // address specified in this statement is the same from which the data is to be received and to which the data is to be sent.
if(status_socket)
{
printf("\n\n\n Socket Connection failed");
}
else
{
printf("\n\n\n Socket Connection completed...");
}
while(1)
{
strcpy(msg1, "AP Message # ");
ltoa(counter1, msg2, 10);
ltoa(counter2, msg3, 10);
strcat(msg1, msg2);
strcat(msg1, " & ");
strcat(msg1, msg3);
status_socket = sl_Send(Sd, msg1, strlen(msg1), 0);
// SL_WLAN_RATE_1M
if( strlen(msg1) != status_socket )
{
printf("\n\n\n All packets could not be sent");
printf("\n");
}
/*
else
{
printf("\n\n\n Packets sent successfully");
printf("\n");
}*/
status_socket = sl_Recv(Sd, RecvBuf, 1460, 0);
if (status < 0)
{
printf("\n\n\nPacket reception failed!!");
}
else
{
// printf("\n\n\n number of packets received = %d", status_socket);
printf(" \n received messages is: %s", RecvBuf);
// printf(" \n ");
// printf(" \n ");
}
counter1++;
if(counter1 == 50000)
{
// printf(" \n received messages is: %s", RecvBuf);
// printf(" \n ");
counter2++;
counter1 = 0;
}
// strcpy(msg1, "AP Message # ");
}
printf("\n\n Out of socket sending and receiving infinite loop!!");
printf("\n\n");
while(1);
}
void mainThread(void *pvParameters)
{
pthread_attr_t pAttrs_spawn;
struct sched_param priParam;
SPI_init();
Display_init();
display = Display_open(Display_Type_UART, NULL);
if (display == NULL) {
/* Failed to open display driver */
while(1);
}
/* Start the SimpleLink Host */
pthread_attr_init(&pAttrs_spawn);
priParam.sched_priority = SPAWN_TASK_PRIORITY;
status = pthread_attr_setschedparam(&pAttrs_spawn, &priParam);
status |= pthread_attr_setstacksize(&pAttrs_spawn, TASK_STACK_SIZE);
status = pthread_create(&spawn_thread, &pAttrs_spawn, sl_Task, NULL);
if(status)
{
printError("Task create failed", status);
}
check_device_initial_mode();
configure_AP_mode();
AP_configuration();
config_network_parameters();
get_device_config_parameters();
do
{
printf( "\n" );
printf( "la la la la" );
printf( "\n" );
}while(retc !=940);
printf( "\n" );
printf( "out of infinite loop!!! " );
printf( "\n" );
ping_first_success();
ping_second_confirmation();
do
{
printf( "\n" );
printf( "Ping Second Confirmation received..." );
printf( "\n" );
}while(flag_second_ping !=1);
unsigned int retc1 = 0;
retc1 = xTaskCreate( socket_task, /* Pointer to the function that implements the task. */
"Socket Task",/* Text name for the task. This is to facilitate debugging only. */
1024, /* Stack depth - small microcontrollers will use much less stack than this. */
NULL, /* This example does not use the task parameter. */
4, // This task will run at Maximum priority.
NULL ); // This example does not use the task handle.
if(retc1 != pdPASS)
{
printf("\n\n");
printf("Socket Task Creation failed!!!");
printf("\n\n");
while(1)
{
;
}
}
if(retc1 == pdPASS)
{
printf("\n\n");
printf("Socket Task Creation Succeeded !!!");
printf("\n\n");
}
while(1);
}
/*
* ======== main_freertos.c ========
*/
#include <stdint.h>
/* POSIX Header files */
#include <pthread.h>
/* RTOS header files */
#include "FreeRTOS.h"
#include "task.h"
/* TI-DRIVERS Header files */
#include "ti_drivers_config.h"
/* TI-RTOS Header files */
#include <ti/drivers/GPIO.h>
extern void * mainThread(void *arg0);
/* Stack size in bytes */
#define THREADSTACKSIZE 1024
/*
* ======== main ========
*/
int main(void)
{
pthread_t thread;
pthread_attr_t pAttrs;
struct sched_param priParam;
int retc;
int detachState;
// Call board init functions
Board_init();
/* Set priority and stack size attributes */
pthread_attr_init(&pAttrs);
priParam.sched_priority = 1;
detachState = PTHREAD_CREATE_DETACHED;
retc = pthread_attr_setdetachstate(&pAttrs, detachState);
if(retc != 0)
{
/* pthread_attr_setdetachstate() failed */
while(1)
{
;
}
}
pthread_attr_setschedparam(&pAttrs, &priParam);
retc |= pthread_attr_setstacksize(&pAttrs, THREADSTACKSIZE);
if(retc != 0)
{
/* pthread_attr_setstacksize() failed */
while(1)
{
;
}
}
retc = pthread_create(&thread, &pAttrs, mainThread, NULL);
if(retc != 0)
{
/* pthread_create() failed */
while(1)
{
;
}
}
/* Start the FreeRTOS scheduler */
vTaskStartScheduler();
return (0);
}
void vApplicationMallocFailedHook()
{
/* Handle Memory Allocation Errors */
while(1)
{
}
}
void vApplicationStackOverflowHook(TaskHandle_t pxTask,
char *pcTaskName)
{
//Handle FreeRTOS Stack Overflow
while(1)
{
}
}
void vApplicationTickHook(void)
{
}
void vPreSleepProcessing(uint32_t ulExpectedIdleTime)
{
}
void
vApplicationIdleHook(void)
{
/* Handle Idle Hook for Profiling, Power Management etc */
}
#if defined (__GNUC__)
void * _sbrk(uint32_t delta)
{
extern char _end; /* Defined by the linker */
extern char __HeapLimit;
static char *heap_end;
static char *heap_limit;
char *prev_heap_end;
if(heap_end == 0)
{
heap_end = &_end;
heap_limit = &__HeapLimit;
}
prev_heap_end = heap_end;
if(prev_heap_end + delta > heap_limit)
{
return((void *) -1L);
}
heap_end += delta;
return((void *) prev_heap_end);
}
#endif
#include <ti/drivers/net/wifi/simplelink.h>
#include <ti/drivers/net/wifi/slnetifwifi.h>
#include <ti/display/Display.h>
#include <ti/drivers/SPI.h>
// TI-Driver includes
#include "ti_drivers_config.h"
#include "pthread.h"
#include "FreeRTOS.h"
#include "Task.h"
#define APPLICATION_NAME ("UDP STA Configuration...")
#define APPLICATION_VERSION ("1.0.0.0")
#define DEVICE_ERROR ("Device error, please refer \"DEVICE ERRORS CODES\" section in errors.h")
#define WLAN_ERROR ("WLAN error, please refer \"WLAN ERRORS CODES\" section in errors.h")
#define SL_STOP_TIMEOUT (200)
#define UDPPORT (1000)
#define SPAWN_TASK_PRIORITY (9)
#define TASK_STACK_SIZE (2048)
#define SLNET_IF_WIFI_PRIO (5)
#define SLNET_IF_WIFI_NAME "CC32xx"
#define SSID_NAME "HCTRIVEDI_AP1" // AP SSID to which the STA is supposed to get connected
#define SECURITY_TYPE SL_WLAN_SEC_TYPE_WPA_WPA2 // Security type could be SL_WLAN_SEC_TYPE_OPEN
#define SECURITY_TYPE_printf "SL_WLAN_SEC_TYPE_WPA_WPA2" // Security type could be SL_WLAN_SEC_TYPE_OPEN
#define SECURITY_KEY "HarshAPConnect" // Password of the secured AP
pthread_t udpThread = (pthread_t)NULL;
pthread_t spawn_thread = (pthread_t)NULL;
int32_t mode;
Display_Handle display;
unsigned char flag_SlWlanEvent = 0;
unsigned char flag_config_nw_parameters = 0;
unsigned char ping_status=0;
unsigned char flag_second_ping = 0;
unsigned char status = 0;
char msg1[26], msg2[6], msg3[6];
extern void echoFxn(uint32_t arg0, uint32_t arg1);
extern int32_t ti_net_SlNet_initConfig();
/*
* ======== printError ========
*/
void printError(char *errString, int code)
{
Display_printf(display, 0, 0, "Error! code = %d, Description = %s\n", code,
errString);
while(1);
}
void SimpleLinkNetAppEventHandler(SlNetAppEvent_t *pNetAppEvent)
{
// unused in this application...
}
void SimpleLinkFatalErrorEventHandler(SlDeviceFatal_t *slFatalErrorEvent)
{
/* Unused in this application */
}
void SimpleLinkNetAppRequestMemFreeEventHandler(uint8_t *buffer)
{
/* Unused in this application */
}
void SimpleLinkNetAppRequestEventHandler(SlNetAppRequest_t *pNetAppRequest, SlNetAppResponse_t *pNetAppResponse)
{
/* Unused in this application */
}
void SimpleLinkHttpServerEventHandler(SlNetAppHttpServerEvent_t *pHttpEvent,
SlNetAppHttpServerResponse_t *pHttpResponse)
{
/* Unused in this application */
}
void SimpleLinkWlanEventHandler(SlWlanEvent_t *pWlanEvent)
{
if(pWlanEvent == NULL)
{
return;
}
switch(pWlanEvent->Id)
{
case SL_WLAN_EVENT_CONNECT:
printf("\n\n");
printf("********************");
printf("\n\n");
printf("Connected to AP with following parameters:");
printf("\n AP SSID: %s",pWlanEvent->Data.Connect.SsidName);
printf("\n Communication Channel: %s",pWlanEvent->Data.Connect.Channel);
printf("********************");
flag_SlWlanEvent = 1;
break;
case SL_WLAN_EVENT_DISCONNECT:
printf("\n\n");
printf("********************");
printf("\n\n");
printf("Disconnected from AP with following parameters:");
printf("\n AP SSID: %s",pWlanEvent->Data.Disconnect.SsidName);
printf("\n Reason for Disconnection: %s",pWlanEvent->Data.Disconnect.ReasonCode);
printf("\n\n");
printf("********************");
break;
}
}
void SimpleLinkGeneralEventHandler(SlDeviceEvent_t *pDevEvent)
{
/* Unused in this application */
}
void SimpleLinkSockEventHandler(SlSockEvent_t *pSock)
{
/* Unused in this application */
}
void Connect(void)
{
SlWlanSecParams_t secParams = {0};
int16_t ret = 0;
secParams.Key = (signed char*)SECURITY_KEY;
secParams.KeyLen = strlen(SECURITY_KEY);
secParams.Type = SECURITY_TYPE;
printf("Connecting to : %s.\r\n",SSID_NAME);
ret = sl_WlanConnect((signed char*)SSID_NAME, strlen(SSID_NAME), 0, &secParams, 0);
if (ret)
{
printError("Connection failed", ret);
}
else
{
printf("\n");
printf("sl_WlanConnect function did not throw any error!! We shall wait for the SL_WLAN_EVENT_CONNECT though!!");
printf("\n");
}
}
void check_device_role(void)
{
if(mode == ROLE_STA)
{
printf("The device is working in STA Mode ...");
printf("\n");
}
else
{
printError("Failed to configure device to STA Role", mode);
}
}
void config_STA_parameters(void)
{
_u8 status = 0; // setup a variable to hold return values...
// set STA Tx power level...
_u8 stapower = 5;
_u8 maxpower = 15;
status = sl_WlanSet(SL_WLAN_CFG_GENERAL_PARAM_ID, SL_WLAN_GENERAL_PARAM_OPT_STA_TX_POWER,1,(_u8 *)&stapower);
if (status != 0)
{
Display_printf(display, 0, 0,"\n\r[line:%d, error code:%d] %s\n\r", __LINE__, status, WLAN_ERROR);
}
else
{
printf("STA Transmit power level configured successfully...");
printf("\n");
printf("STA Transmit power level = %d dBm", (maxpower - stapower));
printf("\n");
}
// set STA Country Code...
_u8* str = "US"; // string of 2 characters. i.e. - "US"
status = sl_WlanSet(SL_WLAN_CFG_GENERAL_PARAM_ID, SL_WLAN_GENERAL_PARAM_OPT_COUNTRY_CODE, 2, str);
if (status != 0)
{
Display_printf(display, 0, 0,"\n\r[line:%d, error code:%d] %s\n\r", __LINE__, status, WLAN_ERROR);
}
else
{
printf("STA country code configured successfully...");
printf("\n");
printf("STA country code = %s", str);
printf("\n");
}
// For changes to take affect, we restart the NWP
status = sl_Stop(SL_STOP_TIMEOUT);
if (status < 0)
{
Display_printf(display, 0, 0,"\n\r[line:%d, error code:%d] %s\n\r", __LINE__, status, DEVICE_ERROR);
}
mode = sl_Start(0, 0, 0);
if (mode < 0)
{
Display_printf(display, 0, 0,"\n\r[line:%d, error code:%d] %s\n\r", __LINE__, mode, DEVICE_ERROR);
}
}
void config_nw_parameters(void)
{
int status_config_nw_parameters = 0;
SlNetCfgIpV4Args_t ipV4;
ipV4.Ip = (_u32)SL_IPV4_VAL(10,1,1,201); // _u32 IP address
ipV4.IpMask = (_u32)SL_IPV4_VAL(255,255,255,0); // _u32 Subnet mask for this STA
ipV4.IpGateway = (_u32)SL_IPV4_VAL(10,1,1,1); // _u32 Default gateway address
ipV4.IpDnsServer = (_u32)SL_IPV4_VAL(8,16,32,64); // _u32 DNS server address
status_config_nw_parameters = sl_NetCfgSet(SL_NETCFG_IPV4_STA_ADDR_MODE,SL_NETCFG_ADDR_STATIC,sizeof(SlNetCfgIpV4Args_t),(_u8 *)&ipV4);
if(status_config_nw_parameters >= 0)
{
printf("\n Network parameters configured successfully and are as follows...");
printf("\n");
printf("IP Address: %d.%d.%d.%d",SL_IPV4_BYTE(ipV4.Ip,3),SL_IPV4_BYTE(ipV4.Ip,2),SL_IPV4_BYTE(ipV4.Ip,1),SL_IPV4_BYTE(ipV4.Ip,0));
printf("\n");
printf("Subnet Mask: %d.%d.%d.%d", SL_IPV4_BYTE(ipV4.IpMask,3),SL_IPV4_BYTE(ipV4.IpMask,2),SL_IPV4_BYTE(ipV4.IpMask,1),SL_IPV4_BYTE(ipV4.IpMask,0));
printf("\n");
printf("Gateway: %d.%d.%d.%d", SL_IPV4_BYTE(ipV4.IpGateway,3),SL_IPV4_BYTE(ipV4.IpGateway,2),SL_IPV4_BYTE(ipV4.IpGateway,1),SL_IPV4_BYTE(ipV4.IpGateway,0));
printf("\n");
printf("DNS Server: %d.%d.%d.%d", SL_IPV4_BYTE(ipV4.IpDnsServer,3),SL_IPV4_BYTE(ipV4.IpDnsServer,2),SL_IPV4_BYTE(ipV4.IpDnsServer,1),SL_IPV4_BYTE(ipV4.IpDnsServer,0));
printf("\n");
}
sl_Stop(0);
sl_Start(NULL,NULL,NULL);
flag_config_nw_parameters = 1;
}
void first_ping_attempt(void)
{
SlNetAppPingReport_t ping1_report;
SlNetAppPingCommand_t pingCommand;
pingCommand.Ip = SL_IPV4_VAL(10,1,1,200); // destination IP address is 10.1.1.200
pingCommand.PingSize = 150; // size of ping, in bytes
pingCommand.PingIntervalTime = 100; // delay between pings, in milliseconds
pingCommand.PingRequestTimeout = 1000; // timeout for every ping in milliseconds
pingCommand.TotalNumberOfAttempts = 20; // max number of ping requests. 0 - forever
pingCommand.Flags = 2; // report at the end of first successful ping
ping_status = sl_NetAppPing( &pingCommand, SL_AF_INET, &ping1_report, NULL );
if(ping_status)
{
printf("\n\r ~~~~~ Ping Failure ~~~~~");
}
printf("\n");
// while(ping1_report.PacketsReceived !=1){}
}
void second_ping_attempt(void)
{
SlNetAppPingReport_t ping2_report;
SlNetAppPingCommand_t pingCommand;
pingCommand.Ip = SL_IPV4_VAL(10,1,1,200); // destination IP address is 10.1.1.200
pingCommand.PingSize = 150; // size of ping, in bytes
pingCommand.PingIntervalTime = 100; // delay between pings, in milliseconds
pingCommand.PingRequestTimeout = 1000; // timeout for every ping in milliseconds
pingCommand.TotalNumberOfAttempts = 50; // max number of ping requests. 0 - forever
pingCommand.Flags = 0; // report at the end of first successful ping
ping_status = sl_NetAppPing( &pingCommand, SL_AF_INET, &ping2_report, NULL );
if(ping_status)
{
printf("\n\r ~~~~~ Ping Failure ~~~~~");
}
printf("\n");
if(ping2_report.PacketsReceived >=45)
{
printf("\n\n");
printf("90%% of the ping response was positive...");
printf("Connection can be assumed rock solid...");
printf("Socket creation and data transfer can be initiated...");
}
flag_second_ping = 1;
}
void socket_task(void *pvParameters)
{
long counter1 = 0;
long counter2 = 0;
_i16 Sd;
SlSockAddrIn_t Addr;
_i8 SendBuf[] = "Hello from STA !!!";
_i8 RecvBuf[1460] ={0};
Sd = sl_Socket(SL_AF_INET, SL_SOCK_DGRAM, 0); // IPv4 socket (UDP, TCP, etc), UDP Packets, Null
if( Sd < 0 )
{
printf("Socket opening failed!!");
}
Addr.sin_family = SL_AF_INET;
Addr.sin_port = sl_Htons(5001);
Addr.sin_addr.s_addr = SL_INADDR_ANY; // bind to any address
// Addr.sin_addr.s_addr = sl_Htonl(SL_IPV4_VAL(192,168,1,31)); // bind to this specific address only.
status = sl_Bind(Sd, ( SlSockAddr_t *)&Addr, sizeof(SlSockAddrIn_t));
if(status)
{
printf("\n\n\n Socket Binding failed");
}
else
{
printf("\n socket binding completed \n");
}
Addr.sin_addr.s_addr = sl_Htonl(SL_IPV4_VAL(10,1,1,200)); // connect with this specific address only.
status = sl_Connect(Sd, ( SlSockAddr_t *)&Addr, sizeof(SlSockAddrIn_t)); // address specified in this statement is the same from which the data is to be received and to which the data is to be sent.
if(status)
{
printf("\n\n\n Socket Connection failed");
}
while(1)
{
strcpy(msg1, "STA Message # ");
ltoa(counter1, msg2, 10);
ltoa(counter2, msg3, 10);
strcat(msg1, msg2);
strcat(msg1, " & ");
strcat(msg1, msg3);
status = sl_Send(Sd, msg1, strlen(msg1), 0);
// SL_WLAN_RATE_1M
if( strlen(msg1) != status )
{
printf("\n\n\n All packets could not be sent");
}
status = sl_Recv(Sd, RecvBuf, 1460, 0);
if (status < 0)
{
printf("\n\n\nPacket reception failed!!");
}
else
{
printf("\n\n\n number of packets received = %d", status);
printf(" \n received messages is: %s", RecvBuf);
// printf(" \n ");
// printf(" \n ");
}
counter1++;
if(counter1 == 50000)
{
// printf(" \n received messages is: %s", RecvBuf);
// printf(" \n ");
counter2++;
counter1 = 0;
}
}
printf("\n\n Out of infinite loop!!!");
printf("\n\n");
}
void mainThread(void *pvParameters)
{
int32_t status = 0;
pthread_attr_t pAttrs_spawn;
struct sched_param priParam;
SPI_init();
Display_init();
display = Display_open(Display_Type_UART, NULL);
if (display == NULL) {
/* Failed to open display driver */
while(1);
}
/* Start the SimpleLink Host */
pthread_attr_init(&pAttrs_spawn);
priParam.sched_priority = SPAWN_TASK_PRIORITY;
status = pthread_attr_setschedparam(&pAttrs_spawn, &priParam);
status |= pthread_attr_setstacksize(&pAttrs_spawn, TASK_STACK_SIZE);
status = pthread_create(&spawn_thread, &pAttrs_spawn, sl_Task, NULL);
if(status)
{
printError("Task create failed", status);
}
/* Turn NWP on - initialize the device*/
mode = sl_Start(0, 0, 0);
if (mode < 0)
{
Display_printf(display, 0, 0,"\n\r[line:%d, error code:%d] %s\n\r", __LINE__, mode, DEVICE_ERROR);
}
switch(mode)
{
case 0:
printf("\n");
printf("Role = STA i.e. Station");
printf("\n");
break;
case 1:
printf("Role = Reserved");
printf("\n");
break;
case 2:
printf("Role = AP i.e. Access Point");
printf("\n");
break;
case 3:
printf("Role = P2P i.e. WiFi Direct");
printf("\n");
break;
case 4:
printf("Role = Role_Tag i.e. Mane pan nathi khabar aa to...");
printf("\n");
break;
default:
printf("Somthing went wrong... No such role defined at SimpleLink Level");
printf("\n");
}
if(mode != ROLE_STA)
{
/* Set NWP role as STA */
mode = sl_WlanSetMode(ROLE_STA);
if (mode != 0)
{
Display_printf(display, 0, 0,"\n\r[line:%d, error code:%d] %s\n\r", __LINE__, mode, WLAN_ERROR);
}
/* For changes to take affect, we restart the NWP */
status = sl_Stop(SL_STOP_TIMEOUT);
if (status < 0)
{
Display_printf(display, 0, 0,"\n\r[line:%d, error code:%d] %s\n\r", __LINE__, status, DEVICE_ERROR);
}
mode = sl_Start(0, 0, 0);
if (mode < 0)
{
Display_printf(display, 0, 0,"\n\r[line:%d, error code:%d] %s\n\r", __LINE__, mode, DEVICE_ERROR);
}
}
check_device_role(); // check device role after configuration..
config_STA_parameters(); // configure STA parameters and restart the device at the end of configuration for the changes to take place
check_device_role(); // check device role after configuration...
config_nw_parameters(); // configure network parameters like IP Address, Gateway, Submetmask etc...
Connect();
printf("returned after connection attempt!!");
printf("\n");
while(flag_SlWlanEvent != 1)
{
unsigned int timer1 = 0;
printf("Waiting for STA to get connected to proposed AP");
while(timer1 != 64000)
{
timer1++;
}
printf("\n");
}
printf("\n\n");
printf("********************");
printf("\n\n");
printf("Connection done successfully... Attempting Ping to AP...");
printf("********************");
printf("\n\n");
first_ping_attempt();
second_ping_attempt();
do
{
printf("\n Second ping confirmation received... Awaiting socket creation...");
}while(flag_second_ping != 1);
unsigned int retc1 = 0;
retc1 = xTaskCreate( socket_task, /* Pointer to the function that implements the task. */
"Socket Task",/* Text name for the task. This is to facilitate debugging only. */
1024, /* Stack depth - small microcontrollers will use much less stack than this. */
NULL, /* This example does not use the task parameter. */
4, // This task will run at Maximum priority.
NULL ); // This example does not use the task handle.
if(retc1 != pdPASS)
{
printf("\n\n");
printf("Socket Task Creation failed!!!");
printf("\n\n");
while(1)
{
;
}
}
if(retc1 == pdPASS)
{
printf("\n\n");
printf("Socket Task Creation Succeeded !!!");
printf("\n\n");
}
while(1);
}
Please let me know if any other information is required on this from my side.
Regards,
H C Trivedi