Hello,
i am working with the AM1808 EVM and the WL1271 board. I am trying to connect to a WLAN network. I am using the WLAN_CU application, scanning is OK and apparently connection to AP is OK, when i check the status of the connection i got:
Status : CONNECTED
MAC: 08.00.28.12.34.56
SSID: LIBERAL
BSSID: 00.24.8c.b0.e8.47
Channel: 10
I am using the AM18x wireless connectivity system test guidelines user´s guide to configure my SUT (system under test). I am running the next commands on the wlan_cu:
• / Privacy Authentication 0 • / Privacy encRyption 1 • / Privacy Wep add 0123456789 1 1 • / Connection Connect YourSSID An this is my AP configuration: