This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220SF-LAUNCHXL: OTA Bad CA file error -456

Part Number: CC3220SF-LAUNCHXL
Other Parts Discussed in Thread: CC3220SF, UNIFLASH

Hello Community,

I am using mqtt_client_CC3220SF example from SDK simplelink_cc32xx_sdk_6_10_00_05 to understand how OTA is working.

I enabled CLOUD_OTA_SUPPORT in ota_setting.h and have compiled the project in CCS and flashed it in debug mode. The userFiles folder contains the certificate files ("digicert_high_assurance_ca.der" and  "RootCACerts.pem") for dropbox and github. I checked if the certificates are valid as well.

 What should be done to avoid this error ?

Thanks and Regards,

Neil