Hi all,
The WL1271 has a dedicated IRQ pin (WLAN_IRQ). This is fine for use in systems where the WL1271 will be connected to the host CPU directly. However in systems where the WL1271 must connect to the host CPU only through a atandard SDIO interface, this could present problems. SDIO multiplexes an IRQ onto SD _DAT[1] line in 4-bit transfer mode.
Questions
- Does the WL1271 support the standard multiplexed SDIO IRQ function, or only a seperate dedicated IRQ pin?
- If WL1271 does not support SDIO IRQ directly already, is there a well-known circuit that can be used to multiplex the dedicated IRQ line onto the SDIO D1 line?
Doug