This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1271 SDIO IRQ

Other Parts Discussed in Thread: WL1271

Hi all,

The WL1271 has a dedicated IRQ pin (WLAN_IRQ).   This is fine for use in systems where the WL1271 will be connected to the host CPU directly.  However in systems where the WL1271 must connect to the host CPU only through a atandard SDIO interface, this could present problems.  SDIO multiplexes an IRQ onto SD _DAT[1] line in 4-bit transfer mode. 

Questions

 - Does the WL1271 support the standard multiplexed SDIO IRQ function, or only a seperate dedicated IRQ pin?

- If WL1271 does not support SDIO IRQ directly already, is there a well-known circuit that can be used to multiplex the dedicated IRQ line onto the SDIO D1 line?

Doug