Hi,
I test 11n Block Ack (BA) feature with WL6/1273 in a product that is WM6.5. I configure all respective parameters of [ "BaPolicyTid_x" , "HT_BA_POLICY_X"] to make the Station as an "BA initiator& receiver" (value of 3).
What I see in wireless-trace is the following: As the Station connects to the AP, it sends a proper Action-frame with BA-initiation to the AP. When the AP replies with Action-frame of "BA success", the Station never hears it (TI FW does not Ack several retries of the AP). Then as AP times out on that Action-frame reply attempts, it then itself initiates a BA session towards the Station (i.e. other direction) and then TI FW does hear it correctly, being the "receiver" of the BA session. Then the session is established ok.
As I saw that issue, I also tested with changing the dot11PowerMode to 1 (CAM), but still the TI-FW does not "hear" the AP's reply to Station's initiation.
So, conclusion is so far I can not make the Station be a successful "BA Initiator"
Is this a know issue ? is the "hearing" problem due to FW being on a different channel at that time? I imagine the FW "must" return to the Serving frequency at the time it should expect the reply (much like it would do when serving actual data ?)
What other configurations shall I try out?
let me know if you want to get a wireless-trace of these experiments.
Thanks,
Ohad.
Motorola Solutions