Hi
in CC3135MOD data sheet, it says that either nRESET (Pin 35) or nHIB (pin 4) can be used for Device Restart and Reset.
So, we have to choose which one (either nRESET or nHIB) we are going to use for Device Restart and Reset.
In order to save the power, we are considering using nHIB for Device Restart and Reset, and want to know if nHIB can not be used for Power On Reset onto CC3135MOD?
During Power ON, only nRESET pin should be held below 0.6V for at least 5ms?
Thanks,