Hi All,
We are using the TI Sitara AM37X Evaluation Module (EVM) Sitara (Win CE 6.0 R3)from Mistral for developing a handheld device
TI WL1271 module is interfaced to the hardware for WiFi functionality.The performance tests for testing the file transfer functionality for a file download from laptop to EVM shows pathetic performance .
The throughput is approximately 1-2Mbps .However iperf shows good throughput(18Mbps). Please let me know if anyone has observed this behavior.
The results repeats if tested on a wired network (eth interface of EVM) .Also the same ftp application and test setup works with good throughput on a competitor platform(EVM replaced)
Thanks,
Jithendran
(Device/Laptop
connected to AP,FTP server running on laptop)
Client application - Customer supplied Kerberos ftp application
Server application - Customer supplied Warftpd