Hi,
We are trying to determine what is the achievable maximum throughput of the TiWi module that is interfaced with the OMAP-L138. Our field testing has demonstrated that we are able to achieve 208KB/s transfer speed using "scp". Now this is very low throughput compared to a DD-WRT (WRT54GL) WLAN test device which can achieve a transfer speed of 2.4MB/s We are hoping that we are able to achieve a comparable rate as to the DD-WRT device we have used for testing.
For this reason, we would like to ask the following to the TiWi Linux WLAN CU development team:
1. Is there an optimal configuration for the WLAN CU that will allow a better throughput that what we are able to achieve?
2. What methods or techniques can we utilize to increase our data throughput?
I appreciate if the team can get back to us quickly.
Cheers,
Grant