Other Parts Discussed in Thread: CC3220SF
Hi,
I was following the "Quick Start Guide" from the documentation that comes with "simplelink_cc32xx_sdk_7_10_00_13".
Following all the steps for IAR i was able to successfully compile the project, but I could not debug it. As recommended I choose the Debugger driver "TI XDS", and on "TI XDS" tab it is selected the "TI XDS110 Emulator".
I already tried with JTAG as recommended which gives me the "Error -2131", and also tried with SWD which gave me the "Error -615".
I also tried the same project but on CCS and everything worked. I have noted that the "Debug configurations" only worked with the "Program" -> "Device" : "Texas Instruments XDS110 USB Debug Prube_0/Cortex_M4_0".
( Do not worked with "Texas Instruments XDS110 USB Debug Prube_0/IcePick_C" nether with "Texas Instruments XDS110 USB Debug Prube_0/CS_DAP".
Can you help me to configure the IAR to be enable debugging the code?
Best regards,
Samuel Simões
For this test I am using the:
Project: "simplelink_cc32xx_sdk_7_10_00_13\examples\rtos\CC3220SF_LAUNCHXL\demos\network_terminal\freertos\iar"
Device: CCS3220SF | CCS3220SF-LAUNCHXL
IAR-ARM: 9.30.1.50054
SimpleLink: simplelink_cc32xx_sdk_7_10_00_13
FreeRTOS: FreeRTOSv202112.00
Emulation package: 9.5.0.00141 | 9.11.0.00128