This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1837MOD: Interface hangs in AP mode

Part Number: WL1837MOD

Hello!

We have WL1837MOD in embedded device using i.MX6 ARM Cortex-A9 CPU.
Linux kernel: 5.4.47
wl18xx: 8.9.0.0.90 
hostapd: TI patched one (c0d9b775e285e0a5ad3c4b7cfe2c5ad7f5adb319)


We are experiencing some issues in AP mode where interface gets in a state where it does not pass IP traffic.
The easiest way to reproduce it is to have multiple clients (like 3) and make them connect connect, get HTTP resource, disconnect. Doing this in loop with 3 clients renders AP unusable in approx. 20 iterations. More clients makes it easier to reproduce. Disable/Enable makes the AP unfreeze. Enabling FULL TI debug logs makes it harder to reproduce (250 iterations might be needed to reproduce).
We tried different network configurations (DHCP, static IP, bridge), different ways to set up AP (hostapd, wpa_supplicant, iwd) and other stuff, and the issue is always reproducible.

wl18xx debug logs
wl18xx-conf.bin