This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPC and DFS controlled by host processor or 1271 / 1273

Hi,

Once 802.11h/SpectrumManagement is enabled for a 127x operated as access point, is the TPC and DFS controlled by software in the host processor, or is it controlled within the 127x radio? (can the 127x device decide to move to a different channel once a radar signal is detected, or does it provide information regarding presence of a radar signal to the host which then arranges with the client to move to a different channel)

Thanks!