Hi
Our system have two antenna, but we find out the transmit by N mode 40MHz only use the same one antenna. can WL1807MOD swithch the antenna? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Our system have two antenna, but we find out the transmit by N mode 40MHz only use the same one antenna. can WL1807MOD swithch the antenna? Thanks.
Hi,
If you are using TI SDK, you can use the configure-device.sh script to modify the wl18xx-conf.bin and switch over to SISO 40MHz. See section 4.1 of this guide: https://www.ti.com/lit/ug/swru561a/swru561a.pdf
If you don't have the configure-device script available, then you can build it as that guide mentions.
Hi,
Thank you for your reply, and sorry for i didn't describe clearly.
example: when we test N mode 40MHz SISO, it transmit from ANT1.Can we switch transmit to ANT2? or it only can using ANT1? Thanks.
Hi Jackie
SISO mode can only be operated by ANT1. It can not be switched.