Part Number: CC3235MODASF
Hello,
I can't seem to find a good description of the recommended layout for the CC3235MODASF. The datasheet includes a section called "10.3.3 CC3235MODAx RF Layout Recommendations", but the information is very limited and I believe it may be incorrect. It shows a 6mm ground clearance from the edge of the module, but this would not fully provide ground clearance under the antenna region (there is 1mm not cleared). I think the 6mm measurement should actually be from the edge of the PCB (not the module). Please see the attached image that illustrates this better.
Also, in the section "10.3.2 CC3235MODx RF Layout Recommendations" for the module without the onboard antenna, it recommends a copper clearance on the top layer under the RF-BG pin. It doesn't recommend this for the CC3235MODASF, but in a separate reference document for the (non-existent?) CC3235MODASF Launchpad layout, this clearance is included. The 6mm antenna clearance also appears to be inline with the correction I mentioned above. Again, please see the attached picture for more details.
Can you provide a better reference layout for this module with more accurate dimensions? Even if the existing drawing is correct, the dimensions reference the module edge which has a +-0.25mm tolerance, which is not ideal for an RF reference.

Thanks,
Ryan