Other Parts Discussed in Thread: CC3220SF-LAUNCHXL, CC3220SF
Hello,
I am trying to connect to Azure Iot Hub with CC3220SF-LaunchXL using iothub_client_sample_mqtt example from azure_cc32xx_4_10_01_01 sdk.
>> ccs version : 12.0
>> simplelink_cc32xx_sdk_4_10_00_07
The callback function for "ReceiveMessageCallback" does not get triggered during the execution of the example. Additionally, the messages are not being sent to the Azure Cloud. The console displays the following message
Starting the iohub_client_sample_mqtt example
Current time: Fri September 19 05:57:20 2023
CC32XX has connected to AP and acquired an IP address.
IP Address: 172.20.10.2
IoTHubClient_LL_SetMessageCallback...successful.
IoTHubClient_LL_SendEventAsync accepted message [0] for transmission to IoT Hub.
IoTHubClient_LL_SendEventAsync accepted message [1] for transmission to IoT Hub.
IoTHubClient_LL_SendEventAsync accepted message [2] for transmission to IoT Hub.
IoTHubClient_LL_SendEventAsync accepted message [3] for transmission to IoT Hub.
IoTHubClient_LL_SendEventAsync accepted message [4] for transmission to IoT Hub.
I tried to update the service pack sp_3.15.0.1_2.0.0.0_2.2.0.7.bin .But this did not solve the problem
Please help me resolve the issue.