This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHCC3235MOD: Using PWM pin on a Mikroe Click Boosterpack 2 with a Mikroe ProFET 15 with i2ctmp sysconfig

Part Number: LAUNCHCC3235MOD
Other Parts Discussed in Thread: SYSCONFIG

I think I made a mistake thinking I could use a Mikroe Click Boosterpack 2 with a Mikroe ProFET 15 as an addon to the LAUNCHCC3235MOD.primarily because the use of the PWM pin to be the output enable on the PROFET 15. That the use hardware in sysconfig list a led, can I share or maybe something else to use without conflict, or is this just not possible with the i2ctmp configuration?

Click BoosterPack 2 — extension for TI LaunchPadTm | MikroElektronika

PROFET Click - 15A (mikroe.com)

Infineon-BTS7004-1EPP-DS-v01_03-EN (mikroe.com)