Part Number: CC3200-LAUNCHXL
Other Parts Discussed in Thread: CC3200, CC3200SDK
I am attempting to setup the CC3200 Launchpad on my second laptop and unfortunately I am getting driver problems. More specifically "Windows cannot load the device driver for this hardware. The driver may be corrupted or missing. (Code 39)":(image 1)
1
Looking deeper, it appears that I have the following drivers: (image 2)
2
Looking back at my first laptop where the drivers are installed properly and are working, this is the setup:(image 3)
3
The windows Code 39 suggested that there were missing or corrupted drivers so I have tried to uninstall drivers, reinstall drivers from the CC3200SDK_1.5.0 and replicate the same situation as on my first computer by transferring the driver files in "Driver File Details" and attempting to install FTDI bus 2.12.28 as in image 3 and still have had zero success and the same error. Any ideas?