This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3230SF: The current consumption of CC3230SF

Part Number: CC3230SF

I am inquiring about the current consumption of CC3230SF.

Please let us know the peak current consumption of CC3230SF during receiving operation and peak current consumption during transmitting operation. Power values are also acceptable.

In addition, we are currently mounting and operating the CC3230SF on a prototype board, and are particularly concerned about the following.
During Wi-Fi reception operation, a peak current of about 350mA is consumed for about 1ms at 8ms intervals.
What is this current consumption? Is it possible to operate without peak current?
The receiving operation is only for DSSS method reception, and is used only for RSSI acquisition purposes.

The following is the current waveform during reception operation