Hello,
does the setting of the country code also affect the (maximum permissible) transmission power?
Best regards,
Roman
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
does the setting of the country code also affect the (maximum permissible) transmission power?
Best regards,
Roman
Hey Roman,
Yes, that is correct. This allows the device to better achieve regulatory compliance for a variety of different regions.
Hello Dylan,
many thanks for your answer.
So the function sl_WlanSet for setting the Tx power, using the parameters SL_WLAN_GENERAL_PARAM_OPT_AP_TX_POWER and SL_WLAN_GENERAL_PARAM_OPT_STA_TX_POWER, will set the Tx power relative to the maximal allowed tx power in relation to the active country setting.
I am right?
The supported transmission power is also included in the WiFi beacons emitted in the access point mode.
Will a change of the Tx power using the function sl_WlanSet, be shonwn in the associated WiFi control beacon information too?
Many thanks again,
Roman
Hello Dylan, many thanks for your answer.
I will check it in the following days and send the result.
Best regards,
Roman