Other Parts Discussed in Thread: CC3200
Hello everyone
I am using the custom board my all example are working properly when i use IC (CC3200) everything is working and wifi is also working. But when i change IC to CC3220S on custom board i am facing problem in Wi-Fi it is not connected and shown this error. Can you please help me.
This Error shown.
Error [-1] at line [84] in function [ConfigureSimpleLinkToDefaultState]
Enter the ssid name to be connected:OnePlus7T
select the security type:
SL_SEC_TYPE_OPEN (0)
SL_SEC_TYPE_WEP (1)
SL_SEC_TYPE_WPA_WPA2 (2)
2
Enter the password for ssid OnePlus7T:12345678
ssid:OnePlus7T passkey:12345678 security : 2
Device IP : 0.0.0.0 , Gateway IP : 10.123.45.1
[WLAN EVENT] Unexpected event [0x30089a]
[WLAN EVENT] Unexpected event [0x30089a]