This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3301: Is there CC3301 fw for the rtos sdio driver?

Part Number: CC3301


Hi

I downloaded the rtos example code for CC3301 , but there is only spi driver in it, no sdio driver. 

Anyway,  I completed the sdio driver by referring to the Linux sdio driver. Now my question is: 

1.  Can the fw in cc33xx_thickmac_package_0_4_0_1.exe support sdio driver?

2. If it can't, can we use the fw in linux sdk to work with rtos sdio driver?

3. If the fw in linux sdk can't be used, can you provide a fw for rtos sdio driver?

This is the file I downloaded:

https://dr-download.ti.com/secure/software-development/driver-or-library/MD-hwSdHCtpQK/0.4.0.1/cc33xx_thickmac_package_0_4_0_1.exe

Thanks