Other Parts Discussed in Thread: CC3235SF
Hello there,
Hopefully an easy question here. I am trying to use Analog input 2 on the CC3235SF eval board. To do this, I pulled up the adcsinglechannel example from the CC32xx sdk. I changed one of the ADC channels configured to use Analog input 2 (P58), and I am getting some weird reading that I was not expecting.
After checking the schematic for the eval board, I am assuming there is a resistor that is DSP? Specifically, I think it is resistor R123. However, I'm not sure how to find this on the eval board, as I can't open the altium files currently.
Am I correct in assuming this is the resistor I need to populate? If so, am I correct that I should use a 0 ohm resistor here?
Thanks,
Greg