This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1837MOD: EAP-TLS and WPA3 support

Part Number: WL1837MOD


- Does WL1837MOD support EAP-TLS in AP or Client mode or both?

- I see R8.9 added WPA3 support with PMF in AP role, is that also supported in Client Mode?

Thanks!

  • Hi,

    • WL1837MOD supports EAP-TLS in station role and it is tested as well. For AP role, we did not test it but since the implementation is on the hostapd and not in the firmware/driver, I expect it would work as well
    • yes, WPA3/PMF is already supported for station role and was added as well for AP role

    Regards,

    Shlomi