Other Parts Discussed in Thread: UNIFLASH, CC3235SF
Hi Ti memers,
We ahe developed a custom board in which we have used cc32335modasf. We programmed it using cc32335sf leaunchpad.
first we programmed it via uniflash to enable developement mode then we programmed the application image from ccs "flash". while flashing from ccs we modified the "image.syscfg", wherein we changed the module type to Antenna module (default was I/C) and then programmed the file. the entire process is ok the application runs fine. But when we power on/off the custom board, the module does not work. we have to reset it externaly by giving low on nReset pin. Just for your reference we have connetced VBAT_RESET to VCC3.3V. We also tried connecting a 100kpullup and 0.1uF cap in nReset pin still the module hangs on power on reset.
If you want for your reference we can share schematic privately