Hi,
We are currently working on the cc3220MODASF launchpad. I attempted to run the adsignalchannel sample code following the instructions in the readme file, but I am unable to properly read the ADC. The output is attached below.
Starting the acdsinglechannel example
ADC0 raw result: 1350
ADC1 raw result (0): 1378
ADC0 convert result: 483626 uV
ADC1 convert result (0): 493657 uV
ADC1 raw result (1): 1646
ADC1 convert result (1): 589665 uV
ADC1 raw result (2): 1656
ADC1 convert result (2): 593248 uV
ADC1 raw result (3): 1646
ADC1 convert result (3): 589665 uV
ADC1 raw result (4): 1652
ADC1 convert result (4): 591815 uV
ADC1 raw result (5): 1656
ADC1 convert result (5): 593248 uV
ADC1 raw result (6): 1655
ADC1 convert result (6): 592890 uV
ADC1 raw result (7): 1658
ADC1 convert result (7): 593964 uV
ADC1 raw result (8): 1658
ADC1 convert result (8): 593964 uV
ADC1 raw result (9): 1654
as per readme instruction out put will 3.3 v but here 0.5 v