Other Parts Discussed in Thread: CC3220R, UNIFLASH
Hi
Have mounted a CC3220S on a PCB where we normaly use CC3220R.
Using the same .sli file. Programming CC3220R works fine but with CC3220S i get FS_ILLEGAL_SIGNATURE.
Can anyone tell me why/what wrong.
/Johan
C:\>SLImageCreator.exe image program --file programming.sli --port COM8
INFO:root:COM PORT COM8
INFO:slbootloader.slbootloader:Connecting to device
INFO:slbootloader.slbootloader:--- Please power off the device ---
Press ENTER to continue
INFO:slbootloader.slbootloader:Power off
INFO:slbootloader.slbootloader:Set break signal
INFO:slbootloader.slbootloader:--- Please power on the device ---
INFO:slbootloader.slbootloader:Power on
INFO:slbootloader.slbootloader:Clear break signal
INFO:slbootloader.slbootloader:Connection succeeded
INFO:slbootloader.slbootloader:Received storage list
INFO:root:Patching RAM...
Preparing...: 100% (10532/10532)INFO:root:Patching SFLASH...
Image Programming: 99% (282624/282688)INFO:slbootloader.slbootloader:Received error : error number = -10363 , extended error = 2633
Traceback (most recent call last):
File "<string>", line 5266, in <module>
File "<string>", line 5262, in main
File "<string>", line 5232, in cmdline
File "<string>", line 4115, in command_image_program
File "<string>", line 2788, in program_image_from_sli
File "<string>", line 2946, in program_image
File "W:\slbootloader\slbootloader.py", line 793, in fs_programming
slbootloader.slbootloader.BootLoaderError:
Error: SLImageCreator.exe: fs_programming error: ret: -10363, ex_err: 2633 - FS_ILLEGAL_SIGNATURE
SLImageCreator returned -1