Other Parts Discussed in Thread: AM62A3-Q1, CC3300, CC3351, CC3350
Tool/software:
Once the driver is compiled, will it load automatically based on compatibility string from device tree? or i have to load it manually?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The firmware gets automatically downloaded so the user does not need to load it manually. For a reference of the device tree, see below:
&sdhci2 {
status = "okay";
bootph-all;
vmmc-supply = <&wlan_en>;
pinctrl-names = "default";
pinctrl-0 = <&main_mmc2_pins_default>;
bus-width = <4>;
non-removable;
ti,fails-without-test-cd;
cap-power-off-card;
keep-power-in-suspend;
ti,driver-strength-ohm = <50>;
#address-cells = <1>;
#size-cells = <0>;
wlcore: wlcore@2 {
compatible = "ti,cc3301";
reg = <2>;
pinctrl-names = "default";
pinctrl-0 = <&main_wlirq_pins_default>;
interrupt-parent = <&main_gpio0>;
interrupts = <72 IRQ_TYPE_EDGE_FALLING>;
};
};will the driver recognize "ti,cc3301"?
I can see it only has "ti,cc33xx" in sdio.c file.
And also in my case driver is not loading automatically. If I load manually also, there is no log.
I am using AM62A3-Q1 processor.
Hi Sathiya,
Are you using a custom board or the AM62A-SK?
"ti,cc33xx" would detect all cc33xx variants (cc3300, cc3301, cc3350, cc3351).
Can you please share your entire kernel boot logs and DTS for review?