Other Parts Discussed in Thread: CC1354P10,
Tool/software:
Dear Sirs:
We are using the LP-EM_CC1354P10_6 together with BP-CC3351.
And we get the software of the MCU from
https://www.ti.com/tool/CC33XX-SOFTWARE
In the past 2 versions(0.6: cc33xx-mcu-plugin-ble and 0.7: cc33xx-mcu-plugin-0.7), the CC33XX-SW — CC33xx restricted software has the support of CC33xx on LP-EM_CC1354P10_6, however, the latest version of the cc33xx_mcu_package_R2 only has the build for the AM243x but no way to build for the LP-EM_CC1354P10.
Besides, the document also has typo as WL18xxEVM is needed.

My question is:
Will TI provide porting to LP-EM_CC1354P10_6 in the future? If the answer is YES, then do you have a schedule? Or I need to do it by myself if I still need to test BP-CC3351 on LP-EM_CC1354P10_6.
Regards,
/ckhsu