This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3301: 802.1k 802.1r WIFI/BT combo IC

Part Number: CC3301

Tool/software:

Hi, 

Could you please suggest a WIFI/BT combo solution with below requirement?

(1) RMII interface

(2) wpa supplicant WPA3 EAP

(3) FIPS

(4) Roaming

(5) 802.1k 802.1r

  • Hi Wayne,

    • Can your customer better specify why is needed RMII interface? What is exact use case
    • Does he looking for SoC which integrate WiFi/Bluetooth/RMII for Etherent PHY and application processor for running own code?
    • Does he need 2.4GHz only or 2.4GHz + 5GHz device?
    • Does he look for TI alternative to ESP32?
    • Does he need low power solution?

    Jan

  • Hello Wayne,

    Can you elaborate if the customer will use a linux or mcu host ?

    Do they want an SoC?

    In short, we do not have a device that covers all of these features, but we do have devices that cover some.

    Our main family of WiFi + BLE devices are WL18 and CC33xx.