This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3351: Is there an option for a Wi-Fi + BLE IC (such as the CC33xx series) with UART interface for the WLAN interface?

Part Number: CC3351
Other Parts Discussed in Thread: CC3120

Tool/software:

Hello,

I am looking to integrate IoT functionality into an exisitng system that only has a UART interface available.

Looking at the  CC3351 chipset and some 3rd party modules this solution looks close to meeting my needs except that this chip and the others I've reviewed use UART to interface with the BLE and some other protocol when interfacing with the WLAN (often SDIO). I was wondering if there are any Wi-Fi + BLE OR Wi-Fi only ics that i could interface to with UART? Or an SoC solution that can support a UART interface with some kind of pass-through operaiton to utilize the WLAN.