This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello expert,
We are in the process of producing a medical device with CC3135MOD.
Since it will be used closer than 20 cm from the human body, we plan to conduct SAR testing.
SAR test center requires us to have continuous transmission.
Is there a setting that allows continuous transmission or a duty ratio close to 100%?
Should I refer to this thread?
I am in charge of electrical circuit design, so if software changes are required, it will take me some time to understand how to set it up.
Sorry, but I would like to explain it to me in simple terms.
Note that 2.4GHz and 5GHz are used.
Regards,
Ryoma
Hey Ryoma,
Yes I would use that other e2e thread as a reference - it seems that customer was able to get through SAR testing using our Radio Test tool.