Other Parts Discussed in Thread: UNIFLASH, MSP432E401Y, SYSCONFIG, TMDSEMU110-U
Tool/software:
Hello,
I recently made a custom board for the CC3235MODASF. I have been struggling to flash or even connect to my device. Here are the relevant parts of my schematic:

I am attempting to connect to the device through the JTAG interface. I am using the XDS110 Rev.A USB debugging probe. The SOP pins are connected to a switch that enables a hardware pullup. I only put one 10kR since it seems that more than one SOP pin will ever need to be pulled high for my use. I believe I followed almost all mandatory design rules as defined within the hardware design checklist. However, I made a mistake. I failed to add 100k resistors to pins 46 and 47 as per instructed. I may have also made a mistake with the nRESET net, but I'm uncertain.
I've tried to use CCS & SYSCFG, as well as UniFlash to program the device. I have tried setting the image.syscfg 'image mode' option to both production and dev with every SOP mode. I have done the same thing in UniFlash. I noticed when using UniFlash, if you select your connection to be the XDS110 debugging probe, any relevant cc32xx device vanishes from the selection menu. Does this mean it is not compatible? I can select it from the menu if the debug probe is not used as the connection interface:


I've probed around the custom board and everything seems to have power and be working properly, apart from the CC3235 itself. Just as a sanity check, I've tried every SOP combination with CCS and UniFlash with the debug header inverted, as well as using a second XDS110 debug probe (I own 3 or 4 of them) and two separate custom PCBs. I've made custom boards in the past with different chips (like the msp432e401y) and have flashed via JTAG just fine.
Are the 100k resistors on pins 46 and 47 required to flash via the JTAG interface? Do you see anything apparent that I've missed?
Any help would be much appreciated,
Dan