This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi everyone,
Is it possible to flash multiple devices simultaneously using the UniFlash CLI? In my specific scenario, the payload is identical, meaning the same firmware will be installed on all devices.
Did you mean that
https://www.ti.com/tool/EMBEDDED-PROGRAMMING
The downloads are not worksing
Hi,
I don't see any issue at my side. Downloads for CC3X00EMBEDDEDPROG and CC3X20EMBEDDEDPROG works properly.
Because you are using CC3220, you should download CC3X20EMBEDDEDPROG .
Jan
i get stucked at this point
"Get Storage List"
After that it does not move
What can be the possible Problem ?
This is the log
This utility programs a binary image to a serial flash connected to CC3120/CC3220 device
Only production devices are supported (i.e. no pre-production devices)
The binary image needs to be prepared in advance using Uniflash utility
Step #1 --> connect to target device
port opened
wait and clear uart rx buffer
set break signal
--- please restart the device ---
wait for ack
receive ack
connection succeeded
get storage list
wait for ack
receive ack
receive storage list
exit bootldr connect
Step #2 --> Reading version info
port opened
wait for ack
receive ack
Reading version info completed
Bootloader version is (3, 0, 1, 0)
It's a CC3220SF device
Step #3 (CC3220 only) --> Switch UART to NWP core
port opened
wait for ack
receive ack
Setting Break Signal
wait for ack
receive ack
Switch to NWP bootloader completed
RawStorageWrite
port already opened
Step #4/8 --> Get SRAM/SFLASH storage info
wait for ack
receive ack
Step #5/9 --> Erasing 3 blocks from SRAM/SFLASH starting from block #0
The process of erasing blocks takes several seconds
wait for ack
receive ack
Status request
wait for ack
receive ack
--- error during raw write
***** Please reset the board and try again *****
---Call Trace:---
File "ImageProgramming.py", line 119, in <module>
File "ImageProgramming.py", line 89, in main
File "ImageProgramming.py", line 62, in BurnImage
---Error Line:---
Traceback (most recent call last):
File "bootldr.pyc", line 455, in RawWrite
File "bootldr.pyc", line 228, in _EraseBlocks
File "bootldr.pyc", line 250, in _check_operation_status
File "serial\serialwin32.pyc", line 260, in write
SerialTimeoutException: Write timeout
This is the parameter when i call
C:\Users\Build-server\Documents\CC3x20_Embedded_Programming_2_0_0\executables\ImageProgramming.exe -p 11 -i C:\Users\Build-server\Documents\Programming.ucf -v
Hi, i ran into another problem. When i use dummy certificate catalog evertyhing is fine. But when i use our own certificate catalog, I am getting error 10246?
Hi,
I am not sure what are you doing. But error code -10246 measn SL_ERROR_FS_DEVELOPMENT_BOARD_WRONG_MAC. That means you are uploading image in development mode with wrong MAC address inside that image. Embedded programming is mainly used for production mode where is no MAC address inside image.
Jan
Hi, i am actually, getting it
error number = -10289 , extended error = 2633
Any help will be greatly appreciated
Hi,
You have issue with signature of your image (-10289 = SL_ERROR_FS_WRONG_SIGNATURE_SECURITY_ALERT).
Do you have programmed your vendor catalogue inside OTP part of SPI flash? Vendor catalogue need to be programmed using Uniflash. But I personally never used vendor catalogue, because I have real code signing certificate from DigiCert.
Jan
Do you have programmed your vendor catalogue inside OTP part of SPI flash?
Yes
In that case, embedded programming is not possible?
I checked that with my certificate catalog i can easily flash with uniflash
"vendor catalogue inside OTP using Unilfash first"
This is already done and works fine. But all the problem are with embedded programming
Hi,
Hard to say what you have wrong at your embedded programming workflow and why you see error -10289. We use embedded programming at our production but with real certificate from CA.
I think you can open new thread with question about embedded programming and vendor certificate. This thread is marked by you as answered already and TI engineers may to have issue to find your question.
Jan