Part Number: CC3230SF
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
In the schematic from the datasheet, there is text that says to add a provision on the board to isolate GPIO01 and GPIO02 while programming. My questions:
1) why do we need to add provision on the board to isolate GPIO01 and GPIO02 while programming?
2) In the schematic, no jumper was added. Do I need to add a jumper to GPIO01 and GPIO02?
3) Does that mean I need to avoid using GPIO21 and GPIO02 and use it when it's absolutely necessary or use it at last when all other GPIOs are used up?