This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3235MODASF: CCS Debugging Questions

Part Number: CC3235MODASF
Other Parts Discussed in Thread: CC3235MODAS, UNIFLASH

Tool/software:

Hello experts,

I have a question about debugging the CC3235MODASF WiFi module.
I am using a prototype board equipped with CC3235MODAS.
And I am using XDS110 USB Debug Probe as a debugger.

When I run debug in Code Composer Studio, I get "Error -1170".
I tried opening the .ccxml for the same project and running Test Connection,
but no errors occurred and the test completed successfully.

The SOP mode of CC3235MODASF is set to "010".
Are there any other steps or settings required to debug with CC3235MODASF?

Details of the error are attached below.



My Code Composer Studio version is attached below.



Best regards
Egawa