We require detailed information about starting the wl1271 using the spi port. My lead engineer says the following:
I have problem with develop low level port for chip wl1271.
Now I try see in linux source code and develop code based on linux code, but when I try initialize and read any bytes using SPI interface,
the chip didn't respond and I do not have any suggestion why. All examples in Internet use only SDIO interface, but for us need SPI interface;
We don't have manuals on chip wl1271, presence of this document would significantly accelerate the development process.
Can we get some documentation or some help?
Kim