Tool/software:
We have experience with CC3220MODASF and have no issues with reaching low hibernate current in production units. Each unit is specifically tested in production to confirm.
We have designed a new product with CC3235MODASF and has very few components besides the module itself. On about half of our recent prototype run the unit hibernate state current is over 200uA. On the other units it's 10uA or less as expected. When we apply some heat to the WiFi module while in hibernate mode the current fluctuates on a 'high current' unit, while on the units with current in the expected range it remains very stable. We are thinking its possible on these high current units the CC3235 is not fully entering hibernate or some aspect of it is not in the correct state. In our testing we are using the same firmware build for the measurements.
Is there something we need to to additionally for the CC3235 when entering hibernate that was not needed on the CC3220? I have re-reviewed the design checklists and other documentation and I can't really find anything different. Is there a way we can pop the shield off the module and check state of signals inside to confirm it is in hibernate or not?
Pete