Tool/software:
Hi , I am using the kernel version "6.1.112" and wireless-regdb package version "2024.07.04" and i am not including the crda package as it is deprecated , i tried to set the regulatory domain using the command "iw reg set US " but when i tried to set it is throwing the error as "cfg80211: loaded regulatory.db is malformed or signature is missing/invalid" as i have checked iam installing the proper regulatory.db and regulatory.db.p7s files in /lib/firmware path but not getting the what is the issue behind this please provide the solution for this any pathches or kernel driver change need to be done it will be helpful . and also i have attached the .config ,defconfig and dmesg for the same which i have used