This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1807MOD: Two simultaneous access points one for 2.4Ghz and one for 5 Ghz

Part Number: WL1807MOD

Tool/software:

Dear team,

I am trying out beagleplay board and checking simultaneous wireless interface

1st interface 2.4 Ghz on wlan0 and 2nd interface 5Ghz on wlan1. But i am not able to run these two simultaneous.

I am able to run two APs simultaneously on either 2.4Ghz with same channel on both hostapd config with separate SSIDs but not able able to run Multi-role - One for 2.4Ghz and one for 5Ghz. 

Is this due to channel restriction to 1? Is it hardware limitation or can be configure via wlconf tool?

iw phy0 info
	valid interface combinations:
		 * #{ managed } <= 2, #{ AP, mesh point, P2P-client, P2P-GO } <= 1, #{ P2P-device } <= 1,
		   total <= 3, #channels <= 2
		 * #{ AP } <= 2, #{ mesh point } <= 1, #{ P2P-device } <= 1,
		   total <= 2, #channels <= 1, radar detect widths: { 20 MHz (no HT), 20 MHz, 40 MHz, 80 MHz }