Tool/software:
My customer has met 3 issues with CC3351:
1. Referring to the command for BLE scanning in CC33xx SDK docs, the server side can send out a broadcast that can be scanned by the phone using the BLE debug assistant, but the device cannot be scanned on another CC3351 (client).
2. Two CC3351, one as 5G AP and the other as client to connect to the AP. The client is constantly pinging the AP, after a long time the network is down. Client side reports "ERROR FW stuck, triggering recovery", after recovery the client can connect to the AP again but reports ERROR FW stuck again after a while. A phone can keep a steady connection to the same AP.
3. CC351 as AP + STA both connected, using STA role to ping the router, the connection is terminated for a short period of time after 10 - 20 minutes. After the disconnection it can recover. This issue does not appear on 2.4GHz band.
Please find the logs for the issues as attached, thanks.
Best regards,
Shuyang